Sensors and Temperature Controllers
![Temperature controller, 24 VA, 0 to 45 °C, blue/black, ECOM0010](/en/images/80d/ECOM0010/95x95/temperature-controller-24-va-0-to-45-c-blue-black-ecom0010.png)
Sensors & Temperature Controllers
Temperature controllers and sensors are generally used to monitor factors relevant to operation and effect. Sensors measure various physical and chemical properties. These may include pressure, motion, brightness, pH levels, and more. Humidity sensors, for example, can detect the moisture level in the air, as well as in building materials or food. Water and water leak detectors belong to the so-called hazard detectors. They indicate when water is leaking. They can be used, for example, to detect malfunctions in washing machines at an early stage. Level monitoring sensors can be used to determine the fill level of containers. Motion detectors also function with a built-in sensor. Controllers, on the other hand, are used not only for monitoring but also for the technical control of physical variables. Temperature controllers have a built-in temperature sensor that detects how high the ambient temperature is. If there is a difference between the desired temperature and the actual temperature, the controller circuit compensates for the difference and brings the environment to the desired degree Celsius. A well-known example of a temperature controller is the thermostat.
Advice on buying sensors & temperature controllers at Bürklin Elektronik
At Bürklin Elektronik you will find a wide range of sensors and temperature controllers. Do you have questions about our product range or individual products? Contact the experts at Bürklin Elektronik with confidence! We will be happy to advise you: [email protected]. You can also find more information in our online magazine.