High quality audio and video cables
Audio and video cables are used where sound and image signals are transmitted to an output device. Mainly, audio and video cables are used in recording studios, in radio, film and TV production as well as in stage and event technology. Special shielding protects the cables from interference from external signals. As a general rule, the longer the cable, the more important this protection is, because the longer the cable, the more likely it is that sources of interference will affect the transmission quality. For this reason, the maximum cable length in the analog transmission range should be between ten and 15 meters. In the digital range, a cable length of up to 20 meters is possible. Depending on the cable, other important parameters must be taken into account. For speaker cables, for example, the cross-section is the most important criterion. High-end versions of speaker cables in our range are convincing in terms of their quality.
Advice from our experts at Bürklin Elektronik
Feel free to contact the experts at Bürklin Elektronik! We will advise you in detail. Write to us at [email protected], or use our convenient call-back service! You can also find more information in our online magazine.