![](https://www.buerklin.com/wp-content/uploads/resized/2023/05/iStock-1054574144-1000x0-c-default.jpg)
Smart Data Integration: Adapters and Connectors for high-performance Networks and Systems
The integration of data in industry has become increasingly important in recent decades. Data is the driving force for the implementation and development of existing and new processes and technologies. They are invaluable to businesses. It is therefore all the more important that data sets can be used efficiently by companies and that flawless data transmission is possible. In our article, you will learn how smart data management is revolutionizing energy supply and how existing systems and networks can be upgraded. We also give you an overview of different types of connectors and adapters.
It is becoming increasingly important for companies to update and upgrade existing data processing systems and thus integrate new technologies into the existing network. Effective connectors and adapters are needed to ensure the compatibility of systems and the connection of individual devices and device parts.
Learn more about high-quality connectors, adapters and the integration of smart data: What special features underlie this topic and which technical components ensure smooth data transmission.
Data is the oil of the 21st century, and data analytics is the internal combustion engine.
– Peter Sondergaard
What is Smart Data?
Smart data offers the potential to solve key challenges of future developments. Smart data focuses on the concept of valuable data, i.e., on the linking of different information to useful content. The motto is: class instead of mass! Consequently, the following questions are central in this context: What value does linked data have for a company, how can it be meaningfully integrated into the value chain?
In order to be able to obtain smart data, it must be cleaned after integration into the system. This means that large volumes of data (from Big Data) must be classified, divided up and reduced. The data becomes valuable when redundancies or contradictions in the data sets are minimized – in other words, when the essence is revealed. Ideally, smart data can be used to predict future scenarios or challenges that can be met with appropriate action concepts.
The bottom line remains: It is necessary to determine and work out how data can be used intelligently to …
- optimize existing processes.
- simplify decision-making.
- improve collaboration between different areas.
This requires high-performance networks for the transmission of data and for the associated technical components.
Smart data management for energy supply
Smart data is basically not tied to one thematic area. Rather, it is a matter of implementing the potential of intelligent information in all segments. One example is the use in energy supply, concerning the topic area Smart Grid.
For the optimization of private consumption of electrical energy, the integration of smart metering is becoming increasingly important – the installation of digital electricity meters for an intelligent electricity network. This allows the connection of energy producers, consumers and energy storage, as well as the exchange of specific status information.
This allows the energy demand to be optimally adapted to the respective situation. For example, in the event of a surplus, the costs for the consumer can be reduced more quickly or fluctuations in the energy supply can be compensated for.
Upgrading and compatibility of existing systems & networks
In order to be able to process the increasing amount of data according to the respective areas of application, regular system upgrades or conversions or upgrades are necessary. Both software and hardware must be upgraded so that the network is not overloaded.
Bürklin Elektronik offers an extensive range of high-quality connectors and adapters so that your demands and requirements for a high-performance network can be met. More information about connectors at Bürklin Elektronik!
Adapters & Connectors at Bürklin Elektronik
Connectors and adapters are electronic components for connecting two devices or parts of devices (for example, circuit boards). Depending on the type of signal that needs to be transmitted, the design of a connector or adapter is subject to specific requirements. For example, a connection with reverse polarity protection or mechanical control must be provided.
The amperage or voltage level are also relevant factors. We provide you with an extensive range of differently designed connectors and plugs in this regard. If, for example, the connector of a monitor or display no longer fits into the new computer, a suitable adapter is needed. This can ensure the connection again and guarantee the compatibility of the systems.
What types of connectors are there?
In connection with the growing diversity of systems, networks and devices, variations of connectors and adapters are also increasingly being produced. For example, there are different connectors for computers, tablets and smartphones – as well as for Ethernet systems and networks. There are also specific connectors, sockets and adapters for use in industry, mechanical engineering and aircraft construction or, for example, in materials handling technology and medical technology.
Overview of connector variations and terminals:
- Data connectors
- Graphic and video connectors
- Serial, parallel and network connectors
- PC internal connectors
- AV connectors
- Low voltage connectors
- Board connectors
- Terminal blocks and rail-mounted terminal blocks
- Industrial connectors
- D-Sub and USB connectors
- Crimp contacts
What types of adapters are there?
There are different adapter designs according to the respective area of application in industry and technology. At Bürklin Elektronik, you will find a wide variety of adapters for your specific area of application.
Adapters at Bürklin Elektronik:
- Audio Adapters
- Bluetooth Hi-Fi Adapter
- Monitor, TV and AV adapters
- Null Modem Adapter (including D-Sub connector)
- USB-Fast-Ethernet-Adapter
- T-adapter
- Display port adapter
Would you like to learn more about the field of connectors? In the magazine article Requirements for Connectors, you will gain informative insights into the requirements that connectors must meet. Or are you interested in 5G and fiber optic networks? Then we recommend you read our informative article on this topic!