Bürklin Elektronik and RAFI - a Success Story for 53 Years
Since the signing of the contract on October 10, 1969, Bürklin Elektronik and RAFI can now look back on 53 years of successful partnership. During this time, with changing economic conditions, political events and, of course, such unforeseeable circumstances as Corona, all the ups and downs have been shaped and overcome in a joint effort. Human cooperation has always been at the heart of everything we do. Trust and exchange naturally provided the basis for mutual success. Even after the recent changes in management, first at RAFI, then at Bürklin, the good spirit was maintained.
We have set ourselves ambitious goals for the future. The new RAFI products that are currently being launched will contribute to our joint success.
Available now at Bürklin Elektronik: RAFI MICON 5 / 5 SL, MICON 5 SAFETY and RACON ST
Revolutionary robustness in miniature format: MICON 5 from RAFI
- Exceptional tactile feedback
- Built-in gold contacts for reliable key operation at low currents
- Extensive range of accessories
- Universal solution for almost all applications
- Various lengths, designs and variants with illumination options to choose from
The perfect choice for demanding environments: RACON ST from RAFI
- Durable contact system
- Wide range of actuating forces
- Operating temperature -40 °C to +125 °C
- Protection class IP67 (front and rear)
- Gold contacts for safe switching at low currents
- Variable mounting heights due to plunger
Press contact
Company address
Bürklin GmbH & Co. KG
Grünwalder Weg 30
D-82041 Oberhaching
Phone: +49 89 55875-0
Fax: +49 89 55875-421
E-Mail: [email protected]
Phone: +49 89 55875-0
Fax: +49 89 55875-421
Email: [email protected]
Phone: +49 89 55875-0
Fax: +49 89 55875-421
E-Mail: [email protected]