RAFI: innovative solutions for 100 years
The history of RAFI began more than 100 years ago. Founder Ernst Bucher and his senior employee and later owner Raimund Finsterhölzl laid the foundation for today's success of the large German company in the first half of the 20th century.
With the production of the first RAFI keyboards and flat input systems, RAFI showed its innovative spirit in the 1970s and 1980s. In 2012, the company set another benchmark with the establishment of its own touch sensor production for capacitive operating systems.
After being acquired by Hoesch AG and subsequently by various shareholders, the company has been owned by the asset management company Oaktree since 2020.
RAFI's products are used in a wide range of industries, including mechanical and plant engineering, as well as domestic installation, electrical engineering and model making.
Product recommendations
Top product categories: Pushbutton switches, tactile switches and emergency stop switches
The pushbuttons, short-travel keyswitches, input keyswitches and emergency stop switches from RAFI are in particularly high demand among Bürklin Elektronik's customers. The manufacturer's quality products impress with their simple operation and high-quality workmanship. The wide range with illuminated, non-illuminated and single or multi-pole models with different contact materials covers all needs.
Pushbutton switches
Pushbutton switches are usually operated manually - ease of operation and fast triggering are of utmost importance. RAFI's pushbutton switches meet these requirements - and more. The first-class pushbuttons and switches are available in various colors, models and designs, and meet the highest quality criteria.
RAFI products are used in electrical engineering, in machine and plant construction, in hand-held operating devices, in controllers and regulators, as well as in industrial robots and in model making.
View pushbutton switches from RAFI
Short-travel key switches and input key switches
Special pushbuttons such as short-travel key switches and input key switches activate or deactivate a circuit or various input forms when pressed. The special feature: after activating the pushbutton, it automatically moves back to the initial position. In special designs, a light element indicates whether the circuit is active.
.RAFI products are excellently manufactured and popular because of their safe and simple operation. Various models guarantee safe switching due to gold contacts - even at low currents. The pushbuttons have excellent tactile and acoustic feedback.
View key switches from RAFI
Emergency stop buttons
The emergency stop button is of particular importance for systems, machines and vehicles: In an emergency, the various devices are immediately disconnected from the mains or put into a safe state by operating the button.
In an emergency, the emergency stop button is of particular importance: In an emergency, the various devices are immediately disconnected from the mains or put into a safe state by operating the button.
Emergency stop pushbuttons from RAFI are available in various designs, as illuminated and non-illuminated models and with various reset functions.

Top products from RAFI
Emergency stop button 1.30.074.521
This RAFIX 16 series product is an illuminated red emergency stop button with a round collar. It is unlocked by turning the mushroom button to the right. In the pressed position, the pushbutton engages positively. Note: Only use universal switching elements!
View product
Pushbutton switch 1.15.106
This 2-pole illuminated pushbutton type RAFI 1.15.106 has a normally closed contact and a normally open contact. The super-bright LED type is thereby permanently installed in the device. The product is fixed with a threaded ring. The pushbutton is mainly used in machine and plant construction, in domestic installations and in model making.
View product
Short-stroke pushbutton 3.14.100.001
The bayable single pushbutton with transparent cover from RAFI is non-illuminated and guarantees safe switching even at low currents thanks to its gold contact. It has a clear button click.
If changeable inscriptions are required or if the overall height of 12.5 millimeters has to be achieved, a button cap can be snapped onto the non-illuminated buttons.
View product
All categories by RAFI